Other Parts Discussed in Thread: UNIFLASH,
Hi all,
I would like to connect IS25LP032D SPI flash on QSPI interface.
Does Uniflash still work with this connection and have no software modification?
Thanks in advance.
B.R.
OC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Naveen,
Thanks so much for your detailed explanation.
After double checked IS25LP032D spec, it supported SFDP command with standard of JEDEC JESD216. And also supported Quad Enable bit set.
My hardware connection should be as below. Please help to double confirm that is ok to work with AWR1642.
|
AWR1642 QSPI Interface |
IS25LP032D |
|
QSPI_CLK (R12) |
SCK |
|
QSPI_CS (P11) |
CE# |
|
QSPI_0 (R13) |
SI |
|
QSPI_1 (N12) |
SO |
|
QSPI_2 (R14) |
WP# |
|
QSPI_3 (P12) |
HOLD |
Thanks in advance.
B.R.
OC