Other Parts Discussed in Thread: AWR1642
Hi,
Today making some measurements by AWR1642 EVM I saw a weird current consumption.
Basically supply the EVM with 5V, current consumption looks like really unstable moving continually between 300mA and 400 mA more or less. (does not metter which AWR configuration I use i.e. 4RX 2TX or 1TX1RX and so on)
Assuming appropriate decoupling capacitors on the EVM , did you never see something like that?
Even because since all the required supply are feeding from 5V I expect more than just 450mA of current comsup.
Please keep in count that I don t have any problem of HW connection between EVM and PC all is working fine using the mmWave Demo Visualizer.
BR,
Fabrizio