Other Parts Discussed in Thread: , LDC2114
Hello,
i have a question concerning scanning four coils, placed one underneath the other with four individual channels.
For example four coils are placed one underneath the other (Every coil on a separate pcb layer).
The four coils are not connected, so it's not a multi-layer coil.
Each coil is connected to one of the channels of the LDC1614 and are scanned one after another.
I've attached a drawing which shows the application.
- How do the coils influence each other?
- Can I detect a deflection of the dome with every channel?
- Can I still detect a deflection if glass is approximately 3 mm thick?
Kind Regards,
Clemens