Other Parts Discussed in Thread: IWR1642, AWR1243
Hi,
I am using IWR1443 and require very high velocity and velocity resolution.
My by calculation, and also confirmed by Sensing estimator, the no of chirps per frame has to be 2600. My questions are as below:
1. The Doxy files says that 'numofLoops' parameter in frame config can have a max value of 255 only. Is this fixed for all devices like AWR1243, and IWR1642 or similar?
2. Can I have multiple chirp loops each having the same configuration. I mean, 16 chirp loops of same configuration, and repeat the chirps for 256 times. There by I actually get 2048 chirps. Is this possible? Will I get what I actually want?
Thanks in advance,
Santhana Raj
PS: The sensing estimator doesn't throw an error on this.