Other Parts Discussed in Thread: AWR1642
Team,
is the AWR1642BOOST a standalone EVM?
Can you clarify the relation to the MMWAVE-DEVPACK and a brief description when the MMWAVE-DEVPACK is needed?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
is the AWR1642BOOST a standalone EVM?
Can you clarify the relation to the MMWAVE-DEVPACK and a brief description when the MMWAVE-DEVPACK is needed?
Thanks
Hello FRAMziskus,
The AWR1642BOOST can work independently and is a standalone EVM.
The MMWAVE-DEVPACK can be used with the mmWave EVMs to enable enable raw capture of ADC data from the front end and evaluation of RF performance and debug.The 2nd CAN connector in case of AWR1642 devices is available on this MMWAVE-DEVPACK. These details are present in the DEVPACK-USERGUIDE
The MMWAVE-DEVPACK is needed to interface with data capture HW like TSW1400EVM.
Thanks,
Raghu
---------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
----------------------------------------------------------------------------------------------------------