Part Number: LDC1000
Hello support team,
I have a question regarding LDC1000.
In case that TBCLK is input from the outside, how do I set PD_CLK (0x05 [0])?
On page 21 of the data sheet (Rev. c), the following is described.
0: CLK_PD
Crystal Power Down.
0: Crystal drive enabled.
1: Crystal drive is disabled. Use this setting to reduce power
consumption with a crystal input when device is in Standby mode.
Use this setting for clock input.
However, in case that the clock is input externally, inductance can not be measured unless PD_CLK is set to 0.
Is the above description wrong?
Best regards,
M. Tachibana