This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Magnitude vs. objects

Part Number: IWR1642BOOST


Hi Experts,

My customer would like to detect a stainless can which is the shape of 20mm height and 5cm diameter by Demo Visualizer.
We have tried but it hardy detects it correctly with high Magnitude.

We have tested the setting as follows:
   FW: V1.01.00.02

 Frame rate    : 5
    Range Resolution : 0.049
 Maximum Unambiguous Range : 5
 Maximum Radial Velocity : 1
 Threshold : 5

1) Could you please let us know the best setting for Demo Visualizer?
2) We would like to know what kind of objects which reflects higher magnitude.   We would like to know the relations among Size, Material, etc.

Best regards,
Hitoshi