Other Parts Discussed in Thread: TMP125
Hi,
We are using TMP123 in our design. Somehow I missed to connect CS# pin to our microcontroller because of GPIO shortage and I directly pulled CS# pin to GND. Now when i am trying to read temperature data the device is not responding. I read in the datasheet that TMP123 requirer 320ms time to start conversion on CS# pin high to low initially.
Can you suggest similar IC with the same foot-print which can work directly with CS# pin low?
Is TMP125 will work on my circuit?