This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: EVM Board LED DS3 turns off during the Demo test

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642

Hi ,

I start by saying that the AWR1642 EVM  already worked by  mmWave Demo Visualizer. I already did   some tests in the past    but unfortunately something happens last week.

Last week I  just powered up the AWR1642 EVB to make some testes but the EVM did not work.

When I push the button on the mmWave Demo Visualizer   "send config to mmW device" the data are sending to the sensor but afterwards I am not able to see any plots.

All HW configurations look like well done and COM ports to transmit and receive data are connected indeed I can read "HW  is connected".

The only different I see between past tests and now is the different LED glowing before  DS4 (NRST) DS2 (5V) and DS3 (NERR_OUT) were turned on instead now DS3 is always turn off, What does it means?

I tried to reboot the device  even the tool  without any changing.

I also re-done the flashing procedure more time (of course appling the jumper on SO2)  but without any results.  

BR,
Fabrizio