Other Parts Discussed in Thread: RF430FRL152HEVM
Hi,
I am doctoral student at Queen Mary University of London. I have recently purchased the TIDA-00524 Ultralow Power Multi-sensor Data Logger with NFC Interface Reference Design.
However, when i got the TIDA-00524, I was unable to find the Coin Cell Battery CR2032 inside it. In addition, I also noticed some other electronic components missing on the board. For instance, D1 and D2. I suppose there are also other components missing too which i need to find out.
Now, I am confused. Which components i need to buy to make these modules functional. For instance, do i need to buy only battery to make TIDA-00524 functional ? Or i require other components as well ? Can someone give me the whole list of components that i need to buy to make these modules functional. Then i can select them from Bill of Materials.
Thanks and Best Regards,
Ahsan