This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AWR1443: waiting for data when setting up with Ubuntu 16.04

Part Number: AWR1443


Tool/software: Linux

I have gone through the instructions for setting up with Ubuntu:

http://processors.wiki.ti.com/index.php/TI_Cloud_Agent

and

http://processors.wiki.ti.com/index.php/Linux_Host_Support_CCSv7

and it all seems to install OK.  When attaching the board with usb, I see:

Bus 001 Device 006: ID 0451:bef3 Texas Instruments, Inc.
which corresponds to the udev rule created in the installation.  I also get serial ports AMC0 and AMC1, as expected
but I don't know which one corresponds to the CFG port and which one corresponds to the DATA port.
I tried both configurations, but the application shows the connection status as "waiting for data" in both cases.
The status lights on the board show as expected:  +5V is red and the yellow "out of reset" light is on.
I tried the chrome version first and then installed the standalone version and got the same results with both.
Here is a screenshot of the demo application page: