Hello, I'd like to connect OPT8241-CDK-EVM to another HSDIO device
what i want is control 9221 with FX2 and Voxel, and only get the OP_Data, CLK(OP_CLK_OUT) and Sync signal(HD_BD_OUT) from J2 connector
However, when I connect EXT_OP_CLK_OUT (pin 6) or EXT_BD_OUT (pin19) to the HSDIO device, the Voxel is shut down and Output data has not printed.
How can I solve this problem? is there any more process to connect J2?