Part Number: TDC1000-TDC7200EVM
Hi. I need to find fluid identification and level codes for TDC1000-TDC7200 EVM. How can i find this txt files? Matt used this files in this video , its links https://www.youtube.com/watch?v=7yoeMxxbl-w
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDC1000-TDC7200EVM
Hi. I need to find fluid identification and level codes for TDC1000-TDC7200 EVM. How can i find this txt files? Matt used this files in this video , its links https://www.youtube.com/watch?v=7yoeMxxbl-w
Thanks.
Here is the config file shown in the video. Keep in mind this is optimized for the specific level/concentration test cell that is used in the video, so it may not be the best settings for your application.
TDC1000_Config0 41 TDC1000_Config1 41 TDC1000_Config2 00 TDC1000_Config3 04 TDC1000_Config4 5F TDC1000_TOF-1 03 TDC1000_TOF-0 FF TDC1000_Error_Flags 00 TDC1000_Timeout 23 TDC1000_Clock_Rate 00 TDC1000_Conts_Trigger 01 TDC7200_Config1 02 TDC7200_Config2 40 TDC7200_Interrupt_Status 07 TDC7200_Interrupt_Mask 07 TDC7200_Coarse_Cntr_Ov_H FF TDC7200_Coarse_Cntr_Ov_L FF TDC7200_Clock_Cntr_Ov_H FF TDC7200_Clock_Cntr_Ov_L FF TDC7200_Clock_Cntr_Stop_Mask_H 00 TDC7200_Clock_Cntr_Stop_Mask_L 00 TRIGGER_UPDATE_FREQ 0004 TDC_AVG/STDEV_NUM_ELEMS 0032 SAVE_GRAPH_DATA_TO_FILE 00 FLOW_MODE_SELECT 00 Y-SCALE_CENTER 0000 X-SCALE_RANGE 0032 MEASURE_RTD1 00 SAVE_RESULT_REGR_TO_FILE 00 GRAPH_MULTI_STOPS 00 TDC_SELECT 00 TEMP_RTD_SELECT 00 TEMP_RTD_MODE 01 TEMP_AVG/STDEV_NUM_ELEMS 000A SAVE_TEMP_DATA 00 GRAPH_YMAX_DATA 0000000000029810 GRAPH_YMIN_DATA 0000000000004E20 TDC1000-HV_DRV_EN1 00 TDC1000-HV_DRV_EN2 00 HV_DRV_EN1_Period 001E HV_DRV_EN2_Period 001E ENABLE_POWER_CYCLE 00 CLK_FREQ_(1-16MHz) 8.000000 CLK_SOURCE_SEL 00 CPU_CLK_FREQ 05 CPU_CLK_EN 00 TDC1000-HV_BST_PWR_EN 00 HV_BST_PWR_EN_Period 0000 FWD2REV_FLOW_DELAY 0000 TDC1000-IMPE_MATCH_EN 00 ENABLE_UART_STREAM 00 ENABLE_MSP430TIMER_TDC 00
TDC1000_Config0 41 TDC1000_Config1 41 TDC1000_Config2 04 TDC1000_Config3 04 TDC1000_Config4 5F TDC1000_TOF-1 03 TDC1000_TOF-0 FF TDC1000_Error_Flags 00 TDC1000_Timeout 23 TDC1000_Clock_Rate 00 TDC1000_Conts_Trigger 01 TDC7200_Config1 02 TDC7200_Config2 40 TDC7200_Interrupt_Status 07 TDC7200_Interrupt_Mask 07 TDC7200_Coarse_Cntr_Ov_H FF TDC7200_Coarse_Cntr_Ov_L FF TDC7200_Clock_Cntr_Ov_H FF TDC7200_Clock_Cntr_Ov_L FF TDC7200_Clock_Cntr_Stop_Mask_H 00 TDC7200_Clock_Cntr_Stop_Mask_L 00 TRIGGER_UPDATE_FREQ 0004 TDC_AVG/STDEV_NUM_ELEMS 0032 SAVE_GRAPH_DATA_TO_FILE 00 FLOW_MODE_SELECT 00 Y-SCALE_CENTER 0032 X-SCALE_RANGE 0032 MEASURE_RTD1 00 SAVE_RESULT_REGR_TO_FILE 00 GRAPH_MULTI_STOPS 00 TDC_SELECT 00 TEMP_RTD_SELECT 00 TEMP_RTD_MODE 01 TEMP_AVG/STDEV_NUM_ELEMS 000A SAVE_TEMP_DATA 00 GRAPH_YMAX_DATA 00000000000128A9 GRAPH_YMIN_DATA 0000000000012845 TDC1000-HV_DRV_EN1 00 TDC1000-HV_DRV_EN2 00 HV_DRV_EN1_Period 001E HV_DRV_EN2_Period 001E ENABLE_POWER_CYCLE 00 CLK_FREQ_(1-16MHz) 8.000000 CLK_SOURCE_SEL 00 CPU_CLK_FREQ 05 CPU_CLK_EN 00 TDC1000-HV_BST_PWR_EN 00 HV_BST_PWR_EN_Period 0000 FWD2REV_FLOW_DELAY 0000 TDC1000-IMPE_MATCH_EN 00 ENABLE_UART_STREAM 00 ENABLE_MSP430TIMER_TDC 00
Also, these have been made with an older version of the GUI. When you load it there may be an error message about a couple of missing fields. Just ignore this, and resave the config file after it has loaded, and it will automatically append the extra fields so the error does not reappear.
Regards,