Hi,
The data sheet for OPT101 states that sensor nonlinearity is typically +/- 0.01 % of FS. Is there any more data that you can supply me with regarding the nonlinearity?
Is the deviation always larger at high input signal or low input signal? Do you have any data regarding how the error is distributed?
The error is given as percentage of FS, the value is measured at 24V supply voltage. Is the deviation (in V) scaled linearily with the supply voltage (i.e. 12V supply voltage leads to half the error in V compared to the error in V at 24V supply voltage)?
Is the linearity error the same in % regardless of if feedback resistor (between "Output"-pin and "-In"-pin) is used or not (i.e. if supply voltage is 24V is linearity expected to be 2,4 mV if no feedback resistor is used, if feedback resistor do lead to 1/2 voltage is the linearity error 1,2 mV)?
The error is given as a typical value, is it possible to say something regarding worst case condition? Are there any measurements regarding spread of error?
In the actual case that I am working with is the ambient temperature stable at 26 *C, and thus are variations due to temperature not of interest.
Thanks in advance for clarification!
best regards
Anders T