Hello,
I was curious as to how the antenna array is designed for 4 chip solution.
The "MIMO Radar" document mentions the basic method of separating the receive antenna by lambda/2 and then separating the transmit antenna by (number of rx antennas) x (lambda/2). So if there are 16 RX antenna, each transmit antenna would be separated by 16 x lambda/2 = 30.57mm. Since there are 12 TX antenna, the board size would at least 340mm, which is unreasonably massive.
I just wanted to see how you guys address this and if you could point me towards some books or any other resources that talk about MIMO antenna placement?
Thank you,
Faiz