My customer want to check if HDC1080 has one issue which presents on SI7020. On SI7020, when the humidity is very to close to 0%, the reading data may jump from 2 to 65534; when it is close to 100%, the data may jump from 65534 to 2. And Silicon Lab's guy told them this is a common issue of this kind of IC. Could you help confirm this? if not like that, it is a good point for us to beat SI7020.