This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: The target is seen in two different azimuth, but at same range when we run mmwave demo project.



Hello,

We have kept the AWR1642device on one vehicle which is not moving. This means sensor is kept at fixed location.  Then we have another vehicle which is approaching the sensor at 30KMPH constant speed from 60m distance. we have collected the plot data and analyzed the detection.  we plotted range vz azimuth and range vs frame number.  we found the single target is coming in two different azimuth with same range.

The same vehicle which is cumming from 60m say in azimuth 0, is also coming in +15 degree azimuth also. both these detection are belonging to same time stamp.

did anyone come across this problem. Please let us know what could be issues.

Regards,

Rajesh