Namaste Reader,
The datasheet of the OPT3001 recommends a 10kOhm pull-up resistor for the SCL and SDA pins.
I'd like to integrate the OPT3001 with the Raspberry Pi 0 W board, which has internal 1.8kOhm pull up resistor on the SCL and SDA pins.
Questions:
1. Would these internal pull-ups be sufficient for a smooth communication between the OPT3001 and Pi 0 W board? What would be the limiting factors in this case of using the existing internal pull-ups?
2. What is the recommended value of external pull-up resistors, considering the fact that two resistors (internal & external resistors) would then result in a parallel combination?
Thank you for reading this post and, for your possible reply.
Thanks | Regards,
Dipen