Other Parts Discussed in Thread: IWR1443BOOST, , IWR1642
Hello,
Our application requires high velocity and fine velocity resolution. Higher than it is possible to set up in the mmWave Demo Visualizer.
I used mmWave Sensing Estimator tool to find and verify our required sensing parameters and estimator says that the parameters are valid.
But when I send the configuration command through the demo visualizer I get the message 'Error-1'.
My questions are:
(1) It is that possible to use this configuration or similar with the Out of Box demo?
(2) If it is not possible to use it with the out of box demo. What is the best way to reach functional solution with the IWR1642BOOST (or IWR1443BOOST) board with required sensing parameters?
Thank you
Pavel

My configuration command:
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 2 1 0
adcCfg 2 1
adcbufCfg 0 0 1 1
profileCfg 0 76 2 6.4 33.73 0 0 3.28 1 79 3000 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 0
frameCfg 0 0 987 0 1000 1 0
guiMonitor 0 0 0 0 1 0
cfarCfg 0 0 8 4 4 0 640
cfarCfg 1 0 8 4 4 0 640
peakGrouping 1 1 1 1 255
multiObjBeamForming 1 0.5
calibDcRangeSig 0 -5 8 256
sensorStart