This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443: radar to measure range to water surface (liquid sensing) from an height of more than 40 m, with angle and SNR information

Part Number: AWR1443


Hello, 

I am looking for a radar that is able to range water surface from a range of at least 40 m, with an accuracy of few cm, providing information about target angle and intensity/SNR for each target. This radar should be implemented on UAVs (drones).

Any suggestion for a radar sensor? What about the AWR1443? Can it detect water up to that range with high resolution?