This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Why Radar Studio captured data "adc_data.bin" always be delayed? Is it a BUG of software?

Part Number: AWR1642BOOST

Hi,

I use AWR1642BOOST and TSW1400 to capture "adc_data.bin" with Radar Studio.

I can get the data successfully, but the problem is that the data captured last time will appear current opratetion.

In the other words, I cannot get the data captured on current round, the data always come from previous round.

Thanks,

Jinjun

  • Hello Jinjun,

    How did you confirm that the data is old data ?

    -Raghu
  • Hi,
    The method is that I test this bug by setting no target and exist target respectively. And I run my matlab code to compute range or angle. The matlab code is verified by lots of data.
    When I take away the target and do the test, and follow TI tutorial to download the data from TSW1400. Then run the matlab code to analyze the range and angle, the result shows me there has a target.
    And go on, I put a target in front of the radar, do the same steps to download and analyze data, the results shows me there has no target.
    Now, when I want to test specific data, I have to repeat the experinment three or five times to confirm the correct data.Because the first time or second time captured may be the old data.

    PS: When I do the test, I choose the clear place without interference.

    Regards,
    Jinjun
  • Hello Jinjun,

    Are you using the HSDC pro directly to extract the adc.bin or using the RadarStudio to get the ADC data ?

    -Raghu
  • Hello Raghu,

    I use RadarStudio to get ADC data, and I don't know how to use HSDC to extract adc.bin directly.

    Jinjun