Other Parts Discussed in Thread: NE555,
Using TMP300 to drive the Reset pin on an NE555. NE555 Reset Pin Iih and Iil are specified as max .4ma. TMP300 Iol is 5ma @ .3V. Reset pin of NE555 has 47K ohm to Vcc pull-up. Circuit is non-functional when connected together. Voltage measurements indicate excessive load on TMP300 . Degraded Voh and Vol voltages on Reset pin. Your comments or suggestions please.