This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300EVM-PDK: AFE4300 software support

Part Number: AFE4300EVM-PDK
Other Parts Discussed in Thread: AFE4300

Hi,

i was using eval kit for AFE4300

Does the source code for AFE4300 eval board & DEVICE GUI (android/windows) is available?

Regards,

Amol

  • Hi Amol,

    The source cod and the GUI installer for the EVM is available at AFE4300EVM's product webpage ( also given below).
    www.ti.com/.../afe4300evm-pdk


    Regards,
    Prabin
  • Hi Prabin,

    We have downloaded & checked the source code from same link, but unable locate the information about following part

    1. initialization of AFE4300

    2. initialization of BCM section (other than weight measurement)

    can you please support on the same

    Regards,

    Amol

  • Hi Amol,

    You can use the AFE4300EVM's GUI to generate the initialization code for the BCM.
    Please use the "Save" tab to save the register settings after you configure the AFE.

    Regards,
    Prabin
  • Hi Prabin,

    We have developed our own hardware using AFE4300 with communication interface with some other micro controller,

    So we are unable to connect our hardware to PC & AFE4300 GUI

    even we are getting the fluctuating ADC values for BCM measurement (21930 & 43945) when we connected dummy 1K resistor between IOUT1 & IOUT0 

    How to verify the output?

    Is there any other method to resolve the issue?

    kindly share the complete source code of TI micro-controller present on AFE4300EVM board, so at least confirm the code implementation

    also, it will be really helpful, if you share the source code for GUI also

    Regards,

    Amol

  • Hi Amol,

    You can run the AFE4300GUI in simulation mode and get the required register setting form the "Low Level Configuration" page after configuring the signal chain.
    AFE4300EVM as well as the GUI doesn't have any initialization inbuilt in them, all the controls are given to the user. So having those source code will not help.
    Regarding the BCM values, is it in FWR mode or IQ mode?

    Regards,
    Prabin