Hello,
DDC264 datasheet defines "INL = ±0.025% of Reading ±1 ppm of FSR" on its1st page, 1ppm of FSR is close to 1LSB, so does it mean it is "±0.025%" error with 1LSB value read out of ADC? I am confused how to make such low and precision input signal to generate 1LSB code. And may I know why define this data?
And there is a figure chat to define full linearity as following, find that INL is worst for the middle level input signal. why is it so big differnce from the both end