This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: If NO PMIC_CLKIN signal and this pin is not grounded, does it impact the performance

Part Number: IWR1443BOOST

In IWR1443Boost schematic, there is no PMIC_CLKIN signal since the resistor R97 is not installed, the PMIC_CLKIN pin also is not grounded as required from PMIC data sheet, does this impact the performance of PMIC?

Thanks!

  • Hello,

    Related to the PMIC using an internal clock (since we are not driving the PMIC_External clock, If the PMIC datasheet (which was released after the EVM) indicates the pin should be pulled to GND,  I would follow the PMIC data sheet.   I have not experienced a PMIC not starting using the 1443 or 1642 EVMs.

    Regards,

    Joe Quintal