i'm interested in evaluating this product for an application that will require 5-6 m range in outdoor conditions.
From the User's Guide (SBOU155B) it states (table 6 about calibration in 'High Ambient') that the Usable range is 1.5 m even if the unambiguous range is 4 m.
My first doubt is whether that usable range only applies to calibration.
Second question is if the outdoor range can be improved by using an IR filter in front of the lens.