Hello!
Tell me where can I model an inductor to detect a metal particle 0.2-0.5 mm (200-500 μm) in size at a distance of 1-10 mm? What should be the coil parameters (diameter, inductance, wire thickness)?
Webench design allows you to calculate the coil, but it does not allow you to specify such a small particle size to get a plot of the dependence of Rp and L on the particle diameter or distance.
How can I understand (model, maybe MS Excell) can I detect such small particles with LDC1000?