Other Parts Discussed in Thread: TMP006
Some questions about TMP007 temperature reading and calibration.
- We use normal mounting before, and now transferred to through hole recently. Normal mounting boards can read real temperature, but through hole can’t, the temperature always higher than real temperature, some accidently a little lower than real temperature. My understanding is the coefficients happen to match with normal mounting in our case, but for through hole, the signal strength is 2x to 3x enhanced, and then has more energy collected in sensors, make more voltage difference and object temperature is calculated higher with the same coefficients, is it right?
- TMP007EasyCal tool can be used to collect and analyze the data, and provide unique calibration coefficients. The coefficient values are programmed in the built-in memory of the TMP007, so it is one time calibration? We never need re-calibrate it if nothing changes (object, distance keep the same). Is it true? Since these data are in TMP007, any system flash memory change such as SW upgrade will not affect the coefficients, is it true?
- How can we get TMP007EasyCal software, is it still available in website?
- How can we use TMP007EasyCal software to analyze the data from TMP006, since TMP006 doesn’t have math engine and nonvolatile memory for storing calibration coefficients, shall we simulate a similar formula as TMP007 and write the coefficients in our FW?
Thanks,
Daisy