I have two questions:
First, the AWR1642 EVM's antennas use immersion silver process, but it is easy to rust,I am ready to use the gold process, so I want to the effect,or is there a better solution?
Second, after the actual test of the AWR1642 board we found that there was a large side lobe in the range of about 1 m, which affected the detection of short-distance weak signals. Do you have any solutions?
Best Regards ,
Monica.Li