This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA460: Transformer equivalent of the TDK B78416A2232A003 part number.

Part Number: PGA460


Hi everyone,

We have to manufacture 6K units of a product with the PGA640 and the transformer TDK B78416A2232A003, but it seems to be that the TDK transformer it is out of stock and the delivery period is very high.

Do you have another equivalent for this part number  TDK B78416A2232A003?

Best regards.

  • Hi Oscar,

    You can find a complete listing of PGA460 compatible/tested transformers on the E2E post "PGA460: Air-Coupled Ultrasonic Transducers & Transformers Listing" at :
    e2e.ti.com/.../620399

    The closest pin-to-pin and identical-performance alternative to the TDK transformer is the Coilcraft WA8351-AL. This part is not yet publicly listed, so you will need to contact Coilcraft directly for samples.