Part Number: OPT8241-CDK-EVM
Is it possible to retrieve/show XY position of a selected pixel in the Watch list using Voxel Viewer v0.9.10? I can see only Z position.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPT8241-CDK-EVM
Is it possible to retrieve/show XY position of a selected pixel in the Watch list using Voxel Viewer v0.9.10? I can see only Z position.
Unfortunately, while the point cloud (x, y, z) data are clearly available, they are not displayed numerically over watch window. This may be a nice feature to have and we will try to incorporate it in next VoxelViewer release. You can however export a point cloud image as PCL file, which gives you the (x, y, z) data in a file, and then you can view it in free PointCloudCompare viewer that permits you to "pick" a point to see its coordinates.
To export PCL file, right-click in VoxelViewer's point cloud window, and then export.
PointCloudCompare can be downloaded here: http://www.danielgm.net/cc/