Hi,
I read the content in the following link:
https://e2e.ti.com/support/sensor/mmwave_sensors/f/1023/p/640548/2363042?tisearch=e2e-sitesearch&keymatch=clutter%20remove#2363042
In this link,Anil says 'Another possiblity is to use the clutter removal function available in SDK 1.1. Note that it will work only if the radar and the clutter is stationary, and the targets are moving. '.If the radar and targets are all moving but they are relative static,under such condition ,does the clutter removal function work?
Thanks in advance.
Regards,
Rata