Part Number: OPT8241-CDK-EVM
I have installed Voxel Viewer 0.9.10 on a Windows 10 machine, connected the OPT8241-CDK board as indicated, turned it on, had a GREEN and BLUE leds (plus the RED on the smaller board) but doesn't stream anything to the Viewer. If I click on 'connect' to a camera, the list is empty. I checked on the connected devices, the devices is seen by Windows. I also tried pressing the reset button with no success. Do I need to install any additional thing?