This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: IWR1443

Part Number: IWR1443BOOST

Tool/software: Code Composer Studio

Hi,

 I'm asking that if the initial phase of every transmitted chirp is the same ? and how can I make them same when transmitting?

Thank you very much

June

  • June,

    A chirp is generated from one of the profiles that are defined by the user at startup. Within each profile, the user has the option to manually phase shift the transmitters. Under the default settings, there is no phase shift for the three transmit antennas and they are the same. However, should you want to change them so they are not the same, you do have the ability to do that too.

    You can experiment with the phase shifting capabilities under our RadarStudio tool that is included in our mmWave Device Firmware Package (DFP).

    The DFP can be found at the link below:

    http://www.ti.com/tool/mmwave-dfp


    Please reply if you have any additional questions.

    Regards,
    Kyle

  • June,

    Did this previous post answer your question? If I do not see a response within the next couple of days, this issue will be considered closed. Please reply if you have any questions.

    Regards,
    Kyle