This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443: CCS/IWR1443

Part Number: IWR1443

Tool/software: Code Composer Studio

Hi All,

My Name is Jean-Paul, From France.

I'm just starting to setup the vital sign demo based on IWR1443 EVM. (Just receved the board 3 days ago !!, so i'm not familiar with all these materials (software and hardware) 

I'm "Strictly folowing" the video to setup the Vital sign demo on my laptop. 

I've sucessfully download the CCS studio V7 and import the Vital Sign CCS on the IDE locally trying to build the project.

Unfortunatly, when trying to build the project I've some errors (24 errors) as follow..

could you help me to solve this issue..

Let me know

is there other way to run the demo (i need to perform a video of the radar results !

Regards

Jean-Paul

see below the compilation results

Description Resource Path Location Type

#137 struct "MMWave_CalibrationCfg_t" has no field "enableCalibration" main.c /vitalSigns_lab line 770 C/C++ Problem
#137 struct "MMWave_CalibrationCfg_t" has no field "enablePeriodicity" main.c /vitalSigns_lab line 771 C/C++ Problem
#137 struct "MMWave_CalibrationCfg_t" has no field "periodicTimeInFrames" main.c /vitalSigns_lab line 772 C/C++ Problem
#137 struct "MMWave_CtrlCfg_t" has no field "freqLimitHigh" sensor_mgmt.c /vitalSigns_lab line 283 C/C++ Problem
#137 struct "MMWave_CtrlCfg_t" has no field "freqLimitLow" sensor_mgmt.c /vitalSigns_lab line 282 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 292 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 336 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 832 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 833 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 834 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 849 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 934 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 942 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 952 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 953 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 969 C/C++ Problem
#137 union "<unnamed>" has no field "fullControlCfg" main.c /vitalSigns_lab line 1091 C/C++ Problem
#20 identifier "MMWave_AdcbufCfg" is undefined main.c /vitalSigns_lab line 288 C/C++ Problem
#20 identifier "MMWAVE_L3RAM_SIZE" is undefined main.c /vitalSigns_lab line 210 C/C++ Problem
#20 identifier "ptrAdcbufCfg" is undefined main.c /vitalSigns_lab line 288 C/C++ Problem
gmake: *** [all] Error 2 vitalSigns_lab C/C++ Problem
gmake[1]: *** [main.obj] Error 1 vitalSigns_lab C/C++ Problem
gmake[1]: *** [sensor_mgmt.obj] Error 1 vitalSigns_lab C/C++ Problem
gmake[1]: Target 'main-build' not remade because of errors. vitalSigns_lab C/C++ Problem
#169-D argument of type "void (*)(uintptr_t, uint32_t)" is incompatible with parameter of type "EDMA_transferCompletionCallbackFxn_t" data_path.c /vitalSigns_lab line 198 C/C++ Problem
#169-D argument of type "void (*)(uintptr_t, uint32_t)" is incompatible with parameter of type "EDMA_transferCompletionCallbackFxn_t" data_path.c /vitalSigns_lab line 547 C/C++ Problem