Hi,
I have doubts on the antenna gain values mentioned across different documents.
1) In AWR1642BOOST datasheet (SWRU508a), on page 12, it is mentioned that "The antenna peak gain is > 9 dBi across the operating frequency band of 76 to 81 GHz."
2)The profile config data structure (rlProfileCfg_t Struct Reference), refers to a variable "rlUInt16_t rxGain" with values from 24 to 48.
My question is, for what value of rx gain in profile config, will I get 9dBi in my AWR1642BOOST board?
I can see obviously, it is not directly mapped. So, I would like to know the relation between the rx gain value set in profile config and the antenna peak gain that I will get?
Or is this a simple case of Tx gain being 9dBi and my Rx gain being any value between 24 to 48dB. Though this explanation sounds reasonable, I have my doubts because, Sensing estimator allows me to set any Tx gain as I desire.
Thanks in advance,
Santhana Raj