Part Number: IWR1443BOOST
Hi Radar Team,
I have a customer who is having issues with their configuration of the Capture Demo project. The task, MmwDemo_dataPathTask, is waiting on handle HWA_done_semHandle, which should ideally be posted when the HWA processing is done but the handle is never received. They are attempting to create the following profile, is it valid?
- Detects objects at 300m range
- Resolves objects spaced 33 cm apart
- transmits just 1 chirp per frame
- In one direction, we transmit just 1 frame
- We obtain a 1024 point FFT
- Since we are not interested in the velocity, number of doppler bins have been pulled down to 1
See below for their chirp config:
- flushCfg
- dfeDataOutputMode 1
- channelCfg 2 1 0
- adcCfg 2 1
- adcbufCfg 0 1 0 1
- profileCfg 0 77 2 3.8 67.92 0 0 7.19 1 1009 15986 0 0 30
- chirpCfg 0 0 0 0 0 0 0 1
- frameCfg 0 0 1 0 2 1 0
- guiMonitor 0 1 0 0 0 1
- cfarCfg 0 2 8 4 3 0 1280
- peakGrouping 1 1 1 1 229
- multiObjBeamForming 1 0.5
- clutterRemoval 0
- calibDcRangeSig 0 -5 8 256
- compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
- measureRangeBiasAndRxChanPhase 0 1.5 0.2
- sensorStart
Let me know your thoughts and if you need any more details.
Thank you!
Barend