Other Parts Discussed in Thread: IWR1642, AWR1443BOOST, AWR1642BOOST, AWR1243
I see the project was done for short range with the IWR1642 but i'm wondering if it can be done or connected to a longer range sensors.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I see the project was done for short range with the IWR1642 but i'm wondering if it can be done or connected to a longer range sensors.
Let's assume 50m.
And assume i got the height to do it since it's outdoor.
I need to detect humans other than actually counting them.
In the 50m range i assume to see 2-3 people max.