Other Parts Discussed in Thread: TIDEP-0092
Hi,
If there are two objects at different angles(one is 0°,the other is 30 °) with the same range in the following:
Is the signal intensity that the radar receives from the two objects identical?My understanding is that the object with higher azimuth has weaker signal intensity, is that right?
Thanks in advance,
Regards,
Rata