HI:
I have to use two AWR1243 for cascade , but the processor has only one MIPI CSI2 interface. i do not konw how can i connect them?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI:
I have to use two AWR1243 for cascade , but the processor has only one MIPI CSI2 interface. i do not konw how can i connect them?
In my design we use two Awr1243, one is master the other is slave. The processor can get the AD data from these Awr1243 in MIPI CSI2 interface. The question is the Processor has only one MIPI CSI2, how to connect to two Awr1243?