This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: flash

Part Number: AWR1642BOOST

hello,

How to solidify the code into the flash in AWR1642BOOST?

Thanks!

  • [2018/2/7 下午12:23:00] [INFO] Cortex_R4_0: Initialization complete.
    [2018/2/7 下午12:23:00] [INFO] Cortex_R4_0: Flashing process starting...
    [2018/2/7 下午12:23:00] [INFO] Cortex_R4_0: Connecting to COM Port COM3...
    [2018/2/7 下午12:23:00] [INFO] Cortex_R4_0: Reset connection to device
    [2018/2/7 下午12:23:00] [INFO] Cortex_R4_0: Set break signal
    [2018/2/7 下午12:23:21] [ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before re-flashing.
    [2018/2/7 下午12:23:21] [ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.
    [2018/2/7 下午12:23:21] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
    [2018/2/7 下午12:23:21] [INFO] Cortex_R4_0: Instance deinitialized!
  • How to generate a valid .bin file in mmw demo?
  • Hi,

    Please review the mmWave SDK User's Guide about information to build the demo. The building process will create two executables: one for the C674x DSP, the other for the ARM R4F. The post building processing step will combine the two files in a single .bin file using the out2rprc.exe utility.

    Thanks
    Cesar
  • Closing the thread due to lack of activity. Please open another if help is still needed.