Other Parts Discussed in Thread: TDC1000, MSP430F5529, TDC7200, MSP430F5528
First post ... so please bear with me :)
[CONTEXT]
I have built an Android application whose focus has so far been sonic (audible) acoustic analysis of wave transmission through solid objects (such as wood, as typically used in musical instruments).
The sonic signals arise from amplified piezo responses to various stimuli that are then fed into the TRRS input of the Android, where analysis is then performed.
The piezo's are simple flat discs and the signals pass thru a straightforward linear preamp.
There are no microcontrollers in this loop (except for the droid, of course).
The amplifier is powered by a 9V battery with a simple toggle switch to avoid drainage.
I wish to extend my application to *Ultrasonic* transduction primarily for the purpose of Speed of Sound determination (as opposed to depth/length determination) of these fixed length solid wooden objects.
My own roundup of TI components that might help me get the job done, and some questions, are ....
[Microcontroller for Android Comms]
It seems that the MSP430 series of boards might be the most suitable for this since OTG is supported out of the box.
The dev kits for this seem to be very well documented and supported.
I should just need to learn my way around programming the MSP unit.
[Transducer Driver]
The TDC range of boards seems to be the right one, but I don't know which model I should choose where the key considerations are
[a] being able to support the necessary voltage/current needs of a transducer placed onto solids of length up to 50 cm
[b] support for (or even has a built-in) Microcontroller (the MSP430 ?)
[c] programmability (is it under direct control of the MSP ?)
[Transducers]
I would like to know how to find a suitable transducer (pair) for this type of application. Cost is always a consideration :)
[Power]
The Ultrasonic assembly should be battery powered (for all of the reasons one might imagine)
Hoping some of you have some time to ponder and help out.
Thanks
Julian