According to page 46 of AFE5803 datasheet, it state that “The VCA wake-up response is typically about 2
μs or 1% of the power down duration whichever is larger. The longest wake-up time depends on the capacitors
connected at INP and INM, as the wake-up time is the time required to recharge the caps to the desired
operating voltages. For 0.1μF at INP and 15nF at INM can give a wake-up time of 2.5ms.”
My understanding is the following.
For power down time up to 200us, power up time is 2 us.
For power down time 200us to 250ms, power up time is 1% of power down time.
For power down time more than 250ms, powre up time is 2.5ms.
Am I correct ?
Thank you in advance.
Auangkun