Other Parts Discussed in Thread: DRV5055, DRV425
Does the sensitivity change in accordance with the magnetic field? Also does the sensor has magnetic offset ? As per my experiments the sensitivity of the sensor is not fixed even for the same conditions and I think there exists some offsets which cannot be eliminated even when calibrated. Also there exits difference between two 5053 sensors. Please correct me if I am wrong.