Hi, I am using IWR1443BOOST with the latest mmwave sdk.
I have ran different labs such as HIgh_accuracy, water and ground, vital sign etc.
I am running Traffic Monitor lab which is having only one step -
Go to traffic Monitor demo and start the MATLAB gui and configure the ports.
Then after configuring the ports and start the project, i got the console output -
Opening configuration file profileTrafficMonitoring.cfg ...
Sending configuration to xWR14xx profileTrafficMonitoring.cfg ...
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1 0
adcbufCfg 0 1 0 1
profileCfg 0 77 300 7 40 0 0 100 1 128 4000 0 0 32
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 32 0 100 1 0
guiMonitor 1 1 0 0 0 0
cfarCfg 0 2 8 4 3 0 1200
peakGrouping 1 1 1 4 224
multiObjBeamForming 1 0.5
calibDcRangeSig 0 -5 8 256
sensorStart
.
But i am not able to get the data/symbol on the screen, i have placed the reflective object in front of the radar but no symbol/data on the GUI.
Any suggestion?
Thanks