Other Parts Discussed in Thread: IWR1443
Dear All,
I have a IWR1443 EVM and the application which I 'm interested in is the Fluid level Application.
The board has been properly flashed and the data are visualized on the https://dev.ti.com/gallery/view/4768107/mmWave_Fluid_Level_Transmitter_1_0_0/
However, I need of some hints for extending the current Demo to my application. In particular, I need to:
- Have the fluid level value available for being sent via internet, or memorized in a data logger, or in a Text file in the PC and so on.
Consider that the tanks are more then one, therefore there is also this problem that ONE pc should manage more than one EVB. - Actually the accuracy and resolution seems to be in the order of 1 mm. I know that this limit is mainly imposed by the operative wavelength of the radiated signal, but there is a method to increase the received information and thus improve accuracy.
- Finally, the tank is very deep (around 25-30m). How can we extend the operative range of the application fluid level.
Many thanks for you kind help and support.
Looking forward to receiving a reply from you,
Davide