Tool/software: Code Composer Studio
Hi
for my application it is very important to get an accurate and fast result from the TDC7200.
Now I ask me, if i get wrong values/glitches and so on, can I handle this wrong value with an interrupt (INTB) to get a new measurement or it is possible to minimze this glitches (see picture below)
and fix the errors in any other way?
pink: in this case is pink an analog Output which shows glitches and wrong measurements through an DAC.
I read in this Forum and in the datasheet that polling the Interrupt status register make more measurement problems and INTB is only to check a Measurement is complete.
But actually i dont use the INTB.
when i Implement the INTB what for advantages i get and can i measure after asking INTB a better accurate frequency?
I used an 8MHz reference clock or the TDC the same oscillator which is used in the TDC7200EVM
my measured frequency is between 400 KHz - 1 MHz
The MSP5529 have an MCU Clock 24 MHZ and SPI 12 MHz
Thanks for help!
greets Ben