This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241-CDK-EVM: Distortion Model for Evaluation Model

Part Number: OPT8241-CDK-EVM


Hi,

I am wanting to get the distortion model of the OPT8241-CDK-EVM, in terms of tangential and radial distortion as well as focal length. Is there a function in the SDK for me to query this? Or is this information otherwise specified in a configuration file or similar?

Thanks,

Tom

  • Hi Thomas, 

    The lens parameters are specified in the configuration files. These files are stored in the EEPROM in the OPT8241-CDK-EVM. You would find these in the "Metrilus Lens Only" profile. 

    You can run VoxelCLI and use profilehwfetch <profileid>. The parameters will be stored in the ~/.Voxel/conf directory. Otherwise, use the "Manage Profiles" section from VoxelViewer, select the Metrilus Lens Only profile and click on the "Copy from Hardware" button.