Other Parts Discussed in Thread: AWR1642, AWR1243
I am looking to estimate the chip limitations at maximum possible chip rates and ranges and would like to get more info about receive (Rx) chain
1) The spec sheet states 5MHz maximum IF bandwidth of the AWR1443 receiver chain but does not specify roll off slope >5 MHz. Clarification would be helpful.
2) Application report SWRA553-May2017 (Programming Chirp Parameters in TI Radar Devices) shows an example of 15MHz maximum beat frequency in the range domain (Table 1. LRR column). How this can be reconciled with 5MHz available IF bandwidth ?
3) The receive IF chain is followed by a digital decimation filter. What is the ADC sampling rate of data going into the filter? Is it programmable or fixed ? If programmable please refer to how-to details.
4) Details on the transfer function (or model) of the two high pass filters in the Rx chain would be appreciated. How the filters behave at high/pass frequencies?
Thank you in advance for comments.