This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: SPI Connection problem when capturing data with the TSW1400

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Hi,

I'm trying to capture raw data from the IWR1443 with the TSW1400.

I'm following the "mmWave sensor raw data capture using TSW1400 board" doc.

Everything goes well until the SPI connection, the connection is failed and SPI connectivity stays red.

I made sure the JP5 jumper is fitted as stated in the common issues section.

I am using EVM with ES2.0 silicon, and the DFP version is 1.0.0.

I have attached the radar studio output log.

Will be glad for some help.

Thanks,

Boaz

GM: Constructor
GM: Tue Feb 20 12:13:25 2018
RSTD.Transmit("/Settings")
[12:13:25]
[12:13:25] ### Running Startup script: "C:\ti\mmwave_dfp_01_00_00_01\rf_eval\radarstudio\Scripts\Startup.lua" ###
[12:13:25] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[12:13:25] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[12:13:25] Scripter ignored: Attempt to UnBuild() again or before Build.
[12:13:25] UnRegisterDll: Ignored. dll "C:\ti\mmwave_dfp_01_00_00_01\rf_eval\radarstudio\Clients\AR1xController\AR1xController.dll" is not registered.
[12:13:25] WARNING:
[12:13:25] RegisterDll: Could not find path "C:\Program Files (x86)\Texas Instruments\RadarStudio\Clients\HSDCPRO\Lua_CS_HSDCPro.dll"
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_dfp_01_00_00_01\\rf_eval\\radarstudio\\Clients\\\\LabClient.dll")
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[12:13:25] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_dfp_01_00_00_01\\rf_eval\\radarstudio\\RunTime\\SAL.dll")
[12:13:25] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[12:13:25] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[12:13:25] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[12:13:25] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[12:13:25] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[12:13:25] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[12:13:25] RSTD.Transmit("/")
[12:13:25] RSTD.SaveSettings(): Settings saved to "C:\Users\boazme\AppData\Roaming\RSTD\config.xml"
[12:13:25] RSTD.Build()
[12:13:25] RSTD.SaveSettings(): Settings saved to "C:\Users\boazme\AppData\Roaming\RSTD\config.xml"
[12:13:25] RSTD.Transmit("/")
[12:13:25] RSTD.AL_Build()
[12:13:25] RSTD.AL_LoadXml()
[12:13:25] RSTD.Transmit("/")
[12:13:25] RSTD.AL_Init()
[12:13:25] RSTD.Clients_Build()
[12:13:25] GM: Init
[12:13:25] GM: Loaded 'C:\ti\mmwave_dfp_01_00_00_01\rf_eval\radarstudio\Clients\\LabClient.dll'
[12:13:25] GM: 1 Guest (s) init
[12:13:25] GM: 1 Module(s) init
[12:13:25] GM: 2 Tab (s) init
[12:13:25] RSTD.Client_LoadXml()
[12:13:26] [RadarAPI]: Starting Matlab Engine..
[12:13:30] [RadarAPI]: Matlab Engine Started!
[12:13:36] [RadarAPI]: ar1.LoadSettings('C:\Users\boazme\AppData\Roaming\RSTD\ar1gui.ini')
[12:13:36] TESTING = false
[12:13:36]
[12:13:36] ***Script completed successfully.***
[12:14:16] [RadarAPI]: Opening Gpio Control Port()
[12:14:16] [RadarAPI]: Status: Passed
[12:14:16] [RadarAPI]: Opening Board Control Port()
[12:14:16] [RadarAPI]: Status: Passed
[12:14:17] [RadarAPI]: ar1.FullReset()
[12:14:17] [RadarAPI]: Status: Passed
[12:14:18] [RadarAPI]: Closing Board Control Port()
[12:14:18] [RadarAPI]: Status: Passed
[12:14:18] [RadarAPI]: Closing Gpio Control Port()
[12:14:18] [RadarAPI]: Status: Passed
[12:14:18] [RadarAPI]: ar1.SOPControl(2)
[12:14:18] [RadarAPI]: Status: Passed
[12:14:31] [RadarAPI]: ar1.Connect(3,115200,1000)
[12:14:32] [RadarAPI]: ar1.Calling_IsConnected()
[12:14:33] [RadarAPI]: ar1.SelectChipVersion("XWR1443")
[12:14:33] [RadarAPI]: Status: Passed
[12:14:34] [RadarAPI]: ar1.SelectChipVersion("XWR1443")
[12:14:34] [RadarAPI]: Status: Passed
[12:14:34] [RadarAPI]: ar1.SaveSettings('C:\Users\boazme\AppData\Roaming\RSTD\ar1gui.ini')
[12:15:12] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_dfp_01_00_00_01\\firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin")
[12:15:12] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[12:16:29] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_dfp_01_00_00_01\\firmware\\masterss\\xwr12xx_masterss.bin")
[12:16:29] [RadarAPI]: Downloading MSS Legacy Binary..
[12:17:19] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[12:17:19] [RadarAPI]: Status: Failed, Error Type: RESP TIMEOUT
[12:17:19] [RadarAPI]: ar1.SaveSettings('C:\Users\boazme\AppData\Roaming\RSTD\ar1gui.ini')